arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All Aqira - Test Data Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Fuselage Shell Testing at IMA Dresden With HBK

IMA, GERMANY

Introduction

IMA GmbH, a company focusing on material research and application technology, has specialized test benches for various airplane and helicopter components, such as fuselages, wings, tail units, and interior components. In the latest generation of IMA Dresden test benches, all measurement data is transferred digitally to data analytics and ensuring real-time control in parallel.

Components for the aviation industry undergo intensive material tests on reaching the prototype stage, and IMA Materialforschung und Anwendungstechnik GmbH in Dresden (IMA Dresden) has been an internationally recognized and accredited partner to the aviation industry in this field for many years. It supports manufacturers and suppliers by providing comprehensive services to prove the durability, function, and safety of components.

As well as simulations, practical component testing is a very important part of IMA Dresden’s work. Not only does the data from Dresden enable suppliers to perform experimental tests on component and structural durability – it also enables comparison with simulations and the verification of the design, repair solutions, joining processes and material selection.

chevron_left
chevron_right

Flexible Equipment for a Varied Range of Measurement Tasks

For the fuselage shell test, IMA Dresden is commissioning a test bench that has been developed from scratch. The design of the servo-hydraulic test bench is a proprietary development borne out of extensive in-house experience, as Gerd Striegler, Head of Measurement Technology at IMA Dresden, explains: “The modified design makes the test bench more flexible for different tests, component dimensions and test standards.” What’s more, several types of stress can be exerted simultaneously and tested in a realistic manner.

The new test bench uses about 30 hydraulic actuators with suitable HBK force transducers, so that it can simulate motion-related tensile, compressive and shear stresses. The reactions to these are measured by 500 strain gauges applied on the test specimen. To achieve this, IMA Dresden relies fully on the QuantumX data acquisition system from HBK for recording the strain gauge signals in various bridge configurations and digitally conditioning them for further processing.

QuantumX is a plug-and-measure solution with comprehensive support of TEDS (Transducer Electronic Data Sheet) technology, which enables fast and flexible adaptation of the test bench in whichever way is needed. The sensor characteristics of each individual sensor are automatically read out from the TEDS chip installed in the sensor or connector, and thus significantly reducing setup times when reconfiguring measurement tasks. Manual entries – frequently the cause of errors – are no longer needed.

Freely Scalable Measurement System

With test benches of this scale, the QuantumX MX1615B, which is far more than just a measurement module, really demonstrates its versatility. The compact design includes 16 measurement inputs with universal channels. The high channel density means the system is freely scalable but also has a smaller footprint. Therefore, each module is flexible and can be distributed as required close to the measurement spots of the test specimen, both as an individual device and interconnected in a large system. In practice, each module can be removed on a day-to-day basis – for small-scale tests, for example – or modules added if more channels are needed.

Christof Salcher, Director Product Management at HBK, names further advantages of this solution: “The individual modules can be used either single or highly distributed and interconnected with a single cable. Synchronous digitization close to the measurement point saves the need for extensive sense leads, enables faster setups and improves signal quality. Together with our catman software it is truly an easy-to-use overall solution solving many testing challenges.”

The modules transmit the data via Ethernet directly to the HBK catman software running on a PC for data visualization, online and post-process analysis, data storage and remote monitoring. For the large test benches commonly used at IMA Dresden, the software also supports visualization on several screens.

Real-Time Control With Maximum Precision

According to Striegler, the biggest advantage of digital data acquisition and processing for IMA Dresden comes in the second stage: “The latest generation test bench uses the measurement data in parallel in real time for test automation.” In structural tests of large components, for applying the load one controller simultaneously actuates several hydraulic actuators. Thanks to real-time control, the controller is able to observe the measurement data during this process, and automatically stop the test or adapt the test program if the data is above or below the set characteristic values.

By contrast, in conventional systems real-time control involves converting the digital measurement data back into analog signals with standardized voltage, and the signals are then fed back into an analog feedback system. A second digitization process is then needed in order for the control system to process the impulses. “In practice, this means that not only is extensive wiring and time needed, but also, above all, the precision suffers,” explains Christof Salcher. “The fully digital measurement and control chain receives the signal in its full quality and can be achieved by using simple Ethernet cables.” Last but not least, using fewer electronics and cables brings considerable cost advantages.

Transparent Configuration, Simple Maintenance

IMA Dresden also benefits from the controller’s direct access to individual sensors. This way, different monitoring parameters can be flexibly adjusted as desired. At the same time, the fully digitized system enables targeted troubleshooting, a faster response time and therefore higher availability of the overall system for demanding testing tasks. The reduced complexity is also evident from the improved maintenance options.

The test bench is managed by the controller system, which communicates synchronously with the QuantumX system via interfaces. The interface technology connects the entire measurement and control chain between the sensors, DAQ system, software and hydraulics control system, in which all components work smoothly together.

Precise Technology for Reliable Digitization

IMA Dresden is gradually digitizing all its test benches and converting them to the new data acquisition method using reliable systems from HBK, says Striegler: “With the new generation of test benches, we are getting an upgrade that scales in line with the more demanding requirements facing both test benches and the measurement tasks.” Another major advantage for IMA Dresden is found in test appliances for mobile and in-field use. The PTP (Precision Time Protocol, IEEE 1588:2008) allows time synchronous data acquisition via Ethernet and creates additional possibilities when working with distributed devices. Real-time Ethernet on the other hand allows low latency real-time communication with limited bandwidth. 

Another key benefit is the standards of the measurement chain elements from HBK, which IMA Dresden has been using for a long time: “In setups as complex as this, the components are generally of different brands,” explains Striegler. “The interfaces of the HBK products and their flexibility enable us to seamlessly connect all the components of a measurement system, and this is especially advantageous when existing test benches get their update for data acquisition one by one.”

About IMA Dresden

IMA Materialforschung und Anwendungstechnik GmbH, or IMA Dresden for short, is an internationally recognized testing, monitoring and certification body for manufacturers and the entire supply industry, helping to get new developments onto the market faster. At two sites in Dresden over a testing area of 10,000 m², innovative products and technologies from industries such as aviation, rail vehicle, automotive, medical engineering, plastics and metal are tested to ensure they are high-quality, reliable and safe. IMA Dresden was founded in 1993 and today has around 240 employees who, with comprehensive engineering expertise, accompany customers through every step of the product development process. Tests range from basic research on small samples to certification tests on complex overall structures. The company develops, tests and creates the technology to perform these tests itself.

More about IMA Dresden

Technology used