arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All Aqira - Test Data Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management
null

How to Select the Right Covering Agent

Selection and Overview of Covering Materials for Your Strain Gauge

 

The quality of a measurement made with a strain gauge essentially depends on the type of installation and design of the measuring point. A thorough preparation of the installation surface, correct connection, and protective covering are important factors for problem-free results.

Immediately after completing the installation of a strain gauge, the measuring point on the surface of the component must be carefully protected from environmental influences by a covering material. In the selection of the covering material, the following factors are to be considered:

  • Environmental conditions during the measurement
  • Duration of the measurement
  • Required service life
  • Measuring accuracy
  • The measuring object must not be stiffened in an impermissible manner; and
  • The material that comes in contact with the measuring point, including the connection cable, must also have a very high insulation resistance and not be capable of triggering any chemical reactions or corrosion.

Condition of Measuring Point

The measuring point must be covered directly after installation. Only the covering materials recommended by strain gauge manufacturers should be used to protect the strain gauge and adhesive layer.

  • The measuring point must be in a perfect condition before being covered—free of dirt, moisture, perspiration from hands, and solder residue. If the strain gauge installation is unavoidable under humid conditions (deadlines, poor weather, humid rooms), the measurement object should be baked dry in an oven, where possible or if this is not possible, the measuring point should be dried using a hair dryer or other devices serving the same purpose.
  • The covering agent must be fully bonded with the area surrounding the measuring point. Defects and capillaries are access points through which aggressive media can enter. The covering agent bond with the surrounding area must remain unchanged during the entire service life of the measuring point. The surrounding area must, therefore, be cleaned as thoroughly as the adhesive point and should reach approx. 1 to 2 cm over the outer adhesive edges. Hand perspiration (fingertips) can cause rust to creep under the covering agent, rendering it ineffective, despite the initial perfect condition.
null
  • The cable entries must be very carefully sealed. The covering agent must surround the wire ends on all sides, including from underneath, to ensure that there are no channels or capillaries through which moisture can penetrate the cover. Embed cable wires individually in the covering agent, in the case of multi-core cables, and cover a part of the cable sheath as well with the covering agent. In critical ambient conditions, roughen the cable insulation first and degrease it with a chemically pure solvent.

Choose the Correct Measuring Point Protection

null

 

AK 22

Viscous putty
Ord. no.: 1-AK22

ABM 75

Aluminum foil with kneading cmpd
Ord. no.: 1-ABM75

NG 120

Nitrile rubber
Ord. no.: 1-NG120

SG 250

Transparent Silicone rubber
Ord. no.: 1-SG250

PU 140

Polyurethane paint
Ord. no.: 1-PU140

SL 450

Transparent silicone resin
Ord. no.: 1-SL450
Temperature range of resistance in air in °C -30°C...+75°C
[-22°F ... +167°F]
-196°C … +75°C
[-321°F … +167°F]
-40°C ... +120°C
[-40°F … +248°F]
-70°C … +200°C
[-94°F … +392°F]
-40°C … +140°C
[-40°F … +284°F]
-50°C … +450°C
[-58°F … +842°F]
Package contents 1 kg 11 pcs.
205 mm x 100 mm
Tube
with 150 g
Tube
with 85 g
3 bottles
each with 30 ml
3 bottles
with 25 g each
One Package sufficient for approx. 30 SG 200 SG 200 SG 20 SG 250 SG 90 SG
Application method Kneading by hand Pressing on by hand Application from tube Application from tube Brush application Brush application
Curing conditions Air drying at room temperature Room temperature Room temperature
… + 80°C
In temperature levels from 95°C - 315°C
Storage life at room temperature 2 years 2 years 15 months 6 months 9 months 6 months
Ingredients Viscous, kneadable, sticky putty 0.05 mm thick aluminum foil coated with 3 mm thick kneading cmpd. Brown, solvent one-component silicone rubber Transparent, solvent free one-component silicone rubber Solvent-containing one component polyurethane paint Transparent, solvent-containing silicone resin
Weather yes yes yes yes yes yes
Water:
Pressurized water
Condensation
Tropical climate
Water vapor
yes
-
-
-
no
yes
-
-
-
condtl.
yes
-
-
-
no
yes
-
-
-
no
yes
-
yes
yes
no
yes
-
-
-
no
Oil:
Engine oil (RT/70°C)
Mineral oil (RT/70°C)
Hydraulic oil (RT/70°C)
no
-
-
-
no
-
-
-
yes
yes
yes
yes
yes
-
-
-
yes
-
-
-
-
-
-
-
Greases - - - - yes -
Solvents in general no condtl. condtl. no - condtl.
Fuels:
Gasoline
Kerosene
no
no
no
no
yes
yes
yes
no
no




Aromatic / Aliphatic mixtures condtl.
Aromatics:
Benzene
Toluene
Xylene
no

no
no
no

no
no
condtl.
no
condtl.
condtl.
no

no
no
no


no
no

no
no
Chlorinated solvents:
Dichloromethane
Carbon tetrachloride
Perchloroethylene
1.2-Dichloroethane
o-Dichlorobenzene
no
no



no
no



no
no
no
no
no
no
no
no



no
no



no
no



Alcohols:
Ethyl alcohol
Methyl glycol
Butyl alcohol
Isopropyl alcohol
Ethylene glycol
condtl.
condtl.



yes
yes



condtl.
condtl.
no
condtl.
condtl.
yes
condtl.
condtl.



no
no



yes
yes



Ketones:
Acetone
Methyl ethyl ketone
condtl.
condtl.
no
condtl.
condtl.
no
no
no
no
no
no
no
no
no
no
condtl.
yes
condtl.
Terpenes:
Dipentenes
Turpentine




condtl.
condtl.
yes






Acids:
Hydrochloric acid conc.
Sulfuric acid 50 %
Acetic acid 50 %
Nitric acid 50 %
Oleic acid conc.
Lactic acid conc.
Air containing acids
no
no
no
no
no


condtl.(1)






condtl.
condtl.

no
no

condtl.
yes
yes
yes
yes
yes


no
no
no
no
no


yes
yes
yes
yes
condtl.
yes


Alkalis:
Sodium hydroxide 10 %
Potassium hydroxide 10 %
Ammonia 28 %
Air containing alkalis
condtl.
condtl.



condtl.(1)




condtl.
no
no

condtl.
no
no



condtl.
no



yes
yes
yes



Liquefied gases (excluding oxygen) - - yes - - -
UV resistance yes yes yes yes yes -

(1) Up to 5 % (destruction of aluminum foil!).

condtl. = Conditionally resistant (at least 10 days at RT)

Combined Agents

A single covering agent is often not enough for sufficient measuring point protection. Examples for combinations of several agents are given by the AK22 and ABM75 (plastic mass plus aluminum foil).

  • In order to add additional mechanical protection to the metal foil, apply an extra layer of materials such as silicon rubber SG250.
  • When producing multi-layer covers, ensure that each layer is fully hardened before applying the next layer. In addition, each layer must overlap the underlying layer by several millimeters on all sides.
  • Frequently, there are several different media acting on a measuring point, such as oil and water. In such cases, for example, oil-soluble ABM75 should be applied directly to the strain gauge, cover with an aluminum foil as a diffusion barrier, followed by an oil-resistant epoxy resin as the final layer.

Multi-layer protection is absolutely essential for indefinable media such as seawater. The top layers that do not come into contact with the strain gauge can be made of other materials from those mentioned here, e.g., asphalt. These materials must, however, not dissolve or chemically change the underlying layers. Apart from that, their electrical insulation resistance is not relevant.

Absolute protection for an unlimited period of time is only possible with a hermetically sealed metallic enclosure. This type of protection can be implemented for standard commercial transducers. However, hermetically enclosing strain gauges for experimental purposes can only be implemented with extremely high overhead or not at all.


Related Products