Force Sensors
HBK Force Sensors and Force Transducers with strain gauge or piezo technology measure static and dynamic tensile and compressive loads - with virtually no displacement.
HORIBA needed to achieve the highest accuracy in torque measurement and the use of the U10M HBK force transducer helped achieve the breakthrough on the VULCAN vehicle test stand.
The HORIBA Group is one of the world's leading providers of automotive testing systems. HORIBA faced a particular challenge during the development of their vehicle test bench VULCAN: How do you achieve the highest accuracy during the measurement of torque - and still ensure an attractive price/performance ratio? International exhaust emission regulations specify standardized driving cycles which can be run on vehicle test benches such as e.g. the "Vulcan" from HORIBA – with the aim of evidencing the performance, emission and consumption patterns of the vehicle. The test bench uses drives to simulate realistic loads such as slopes, inclines or level roads.
HORIBA's vehicle test bench VULCAN has just one motor per axle, located between the drive rollers. The result is shorter shafts and therefore an improved dynamic behavior. The torque of an axle is recorded via a single force transducer, with the reaction torque of the motor imparting the force to the force transducer via a lever.
A key factor for reproducible results here is the most accurate determination of the torque on the drive. The accuracy of the entire system is dependent on the metrological properties of the transducer used because the torque is a product of force times lever arm. If the results of the transducer are imprecise, the meaningfulness of the entire test on the vehicle test bench could be in question.
HORIBA therefore places maximum value on maximum accuracy, far better than 0.1% – and finally found the route to success in a simple and clever modification of the measurement process. In addition to a constructive modification, the use of the U10M HBK force transducer helped with the breakthrough.
The force transducer U10M is thereby calibrated in the application, where its excellent reproducibility is an advantage. The U10M has a vibration bandwidth of 200% maximum capacity and works reliably in dynamic operation up to the nominal force. Manufactured from rustless material and protected to IP67, the U10M - HORIBA impresses with its dynamic properties, reliability and precision.
Installation of U10M on the motor that also simultaneously functions as a brake. Force is applied via the lever.
U10M HBK force transducer
The example shows: Every test bench is only as good as the measurement technology used in it. The accuracy and reliability of measurement results from the transducer used is decisive for the meaningfulness of the tests carried out at a later date. With a wide product portfolio, ranging from sensors to measurement electronics to software, HBK offers solutions for all types of tasks and enables better results in test benches.
The Company manufactures and sells automotive emission measurement systems, environmental measuring instruments, wide range of scientific analyzers, and medical diagnostic analyzers, and measuring equipment used in the semi-conductor industry. HORIBA also manufactures and markets peripheral measuring and analysis devices. Moreover, the Company equips such facilities as laboratories with measuring and analytical equipment for R&D, production, and other applications.
HBK Force Sensors and Force Transducers with strain gauge or piezo technology measure static and dynamic tensile and compressive loads - with virtually no displacement.
HBK weighing technology is synonymous with precision, safety, dependability, and quality since our load cells have set the standard for decades. The brand stands for innovative capacity, flexible and cost-effective solutions that meet virtually any customer requirement. We are also committed to the promotion and advancement of hygiene in relevant industries.
HBK provides a wide range of load cells, strain gauges and transducers. The quality of our products is renowned worldwide and is the result of our unique experience and knowledge in the production, and development of our products. Find out all our measurement solutions.
The Novares Group looks beyond the current crisis to a future with a V8900 HBT1220 shaker from HBK.
The technical complexity and regulations relating to noise and vibration of machinery and ships demand the latest technology
BATZ uses HBK equipment for testing according to its customers’ requirements
Crown Equipment Corporation explored how improving the sound of their forklift trucks could create a better product and a more satisfying user experience
Ground Vibration Tests Prove to be a Key Milestone for NASA’s X-57 Maxwell
New ChovACUSTIC systems leverage all the benefits of state-of-the-art sound level meters
Controlling noise and vibration in the railway sector is key for the well-being of residents and passengers alike
To decrease the hours spent driving between fields during harvest time, New Holland reduced the pass-by noise of machines, gaining a higher road speed rating.
Acciona Infrastructure needed to increase competences and offerings for building acoustics and sound insulation, Brüel & Kjær provided the solution.
Air France Case Study highlighting how Air France - a major player in engine MRO - optimized their Zephyr test bench using B&K Tescia Repetitive Testing System.
Noise control: When it comes to environmental noise, Gießen Regional Council and HBK are listening very carefully
Case Study featuring Lockheed Martin and how Brüel & Kjær helped test different variants of the F-35 jet with the aim of protecting ground crews from noise exposure and increasing the durability of the jets.
Gorenje wanted to increase their R&D efficiency with a faster acoustic characterization system. And they turned to us
After Airbus modified the A330 to create the military version, they needed to update the aircraft’s noise certification so it could still use civilian airports.
The French aerospace research centre, ONERA, has acquired a 200-channel Brüel & Kjær PULSE™ acoustic data acquisition system for wind tunnel testing.
Aircraft manufacturers have been approved to use PULSE for aircraft noise certification according to international standards.
Dassault Aviation has performed noise certification tests on their new Falcon 8X business jet, using an acoustic data acquisition and analysis system from Brüel & Kjær.
Airbus has acquired a 250-channel Brüel & Kjær PULSE™ data acquisition system for multi-purpose noise and vibration testing.
Engineering consultancy company ATA Engineering, Inc (ATA) has strengthened its ties with instrument and solution provider, Brüel & Kjær, with the procurement of a PULSE Data Acquisition and Analysis system.
Brüel & Kjær is to supply Pratt & Whitney with a Static Engine Certification Test (SECT) System.
Brüel & Kjær recently delivered their HVME (Hull Vibration Monitoring Equipment) solution to BAE Systems Submarine Solutions.
Airbus Defence and Space and Brüel & Kjær have successfully completed noise measurements on the Eurofighter jet, to calculate its on-ground noise exposure under different thrust and flight configurations.
Brüel & Kjær has been selected by Dassault Aviation to provide high-pressure surface microphones for the development of the nEUROn experimental Unmanned Combat Air Vehicle (UCAV).
Aerospace leader Lockheed Martin has expanded its vibration measurement capabilities for testing satellite systems, with a 450-channel PULSE™ vibro-acoustic data acquisition system.
Collaboration with Airbus Defence & Space will model sound for low-noise flight plans
To ensure high quality and increase production yield, Volkswagen contacted Brüel & Kjær to equip DISCOM Production Testing System to pinpoint the root causes.
To minimize errors and reduce setup time, automotive seating manufacturer, Faurecia, uses the Transducer Smart Setup app for modal measurements.
The challenge car makers face every day is designing cars to withstand all possible use cases during their entire product lifecycle. To support these investigations, Stellantis uses nCode DesignLife software within their development processes for fatigue analysis.
With a wide range of sound measurement tasks, VM Acoustics needed a measuring instrument, that could serve all their needs reliably.
HBK’s Engineering Solutions embarked on the challenge of developing a common Failure Reporting, Analysis, and Corrective Action System (C-FRACAS+) for NAVAIR Command’s 33 programmes, each comprising diverse aircraft and systems with unique data requirements.
HBK's Advanced Material Characterisation & Testing facility in the UK, has helped accelerate NIO's fatigue simulation capabilities through a unique combination of bespoke testing solutions to provide high quality material fatigue data and the power of nCode software.
Once a year in the Lost Village revellers gather to immerse themselves in four days of live music and festivities. HBK, in agreement with the local authority and with the help of Noisy’s noise monitoring platform connected to B&K 2245 sound level meters, reduced the sound levels, resulting in very few noise complaints over the weekend.
Field report from ETH Zurich as part of the eXact project。