arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Too much fertilizer? A globally unique test bench for investigation and analysis

cemagref, france

Introduction

Cemagref, the French Institute for Agricultural and Environmental Engineering Research is a specialist in spreading fertilizer at one of its nine sites in Montoldre. The equipment to chart the spread of the fertilizer as it is ejected by centrifugal spreaders of mineral fertilizer, is globally unique.

chevron_left
chevron_right

Investigating fertilizer spreading: the limits of the current system of evaluation

Up until 2006, the amount of fertilizer that was spread was expressed as the transverse distribution to the axis of progression of the machine in a complete pass. As an already integrated outcome was provided, extensive analyses were required to optimize the spread of the fertilizer and thus minimize environmental pollution. But increasing the power of the fertilizer spreader produced so many set points that it became virtually impossible to optimize the machines without having recourse to models of the spread, created under real conditions. So the conventional test bench was inadequate for future requirements.

A revolutionary test bench principle

Fertilizer spreaders distribute fertilizer via two spinning disks, ejecting the fertilizer backwards and sideways out of the machine. The distribution over the soil corresponds to a circular layer of varying density. The control station, for which Cemagref has applied for a patent, works on the basis of radial measurement of the distributed quantities: During a spreading test, the machine is set to rotate around itself. The distributed layer is charted for each angular sector by receiving containers arranged radially around the center of rotation. The result is the actual distribution of the fertilizer on the soil. There are several data processing phases as first, the spread is characterized and then a model of the distribution over the soil is created. Academics and engineers can then work with objective measurement results and are no longer dependent on bold interpretations. This technical innovation also has a practical advantage: at 40 m x 1 m, the place where the test bench is installed is 15 times smaller, which makes it far more economical. 80 load cells with a measuring range of up to 1 kg weigh the quantities of fertilizer received by the 80 containers. All the load cells are continuously and synchronously interrogated with the aid of MGCplus at a frequency of up to 2400 Hz. The obtained resolution of 0.02 g allows the mass accumulation in each container to be measured by the grain. The simultaneous measurement of the relative angle of the centrifugal fertilizer spreader in relation to the series of containers allows the average fertilizer density to be derived in each physical

position of the layer. The chart made of the layer spread over 220° takes one to three minutes, depending on the measurement accuracy required. Three RTN load cells with a measuring range of up to 2.2 t allow simultaneous measurement of the complex made up of revolving support, fertilizer spreader and fertilizer. The loss in weight is measured continuously at a resolution of 20 g. This allows the flow to be recorded at the outlet of the fertilizer spreader.

 

Easy data acquisition with MGCplus and catman®

All the load cells used are calibrated or simply tested remotely, without the need for adjustments to be made on the test bench itself. Because there is a direct connection to the MGCplus amplifier system and a useful calibration window in the catman® software, amplifications and offsets are simply adjusted. The recordings of the load cells used guarantee that sequences can be retraced. A series of catman® display windows allow the measurement data of all the load cells to be monitored in real time. The program supports links to other programs (database, processing software) and no intervention is required from the user. Thanks to this technology, a new and full test (parameterization, test, saving and processing the data) can be run every five minutes.

Related Products

No more result to load