arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Aqira - Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All Aqira See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management
null

How to Select the Right Adhesive for your Strain Gauge Installation

Task and Function of the Bonding Material

 

The bonding materials have the task of firmly attaching the strain gauge to the measured object’s surface and transferring the object’s deformation without loss to the strain gauge. The various conditions, influences, and application options, require different bonding materials and installation methods. Bonding is the most important factor.

The particular advantages of this connection method, with regard to strain gauge installations, are as follows:

  • The possibility of connecting different materials, even dissimilar ones. The connection is implemented at room temperature or higher temperatures, depending on the type of adhesive.
  • It has no influence on the materials which are to be connected (however, some restrictions may apply for plastics).
  • Chemically-hardening adhesives (these are only still used in strain gauge technology) are characterized by low moisture absorption rates.
  • Control of working speed through the selection of different adhesive types or curing conditions (hot or cold curing).
  • Higher specific electrical resistance contributes to higher insulation resistance between the strain gauge and the component.

Types of Bonding Materials

Both the working conditions at the installation site, and the various requirements for the bonding material performance, particularly in regard to the operating temperature, have led to the availability of various types of bonding materials. Bonding materials can be differentiated as follows regarding the application technology.

1. Cold-curing Adhesive

These can be easily applied and do not require much effort. There are single-component adhesives that start curing with appropriate humidity as well as two-component adhesives that must be mixed before application. Adhesive with very short reaction times are also called “superglues”. They are applied preferably in experimental tests.

2. Hot-curing Adhesives

These adhesives can only be used if the test object can be brought to the required curing temperature. This is generally possible in transducers manufacturing, but also where strain gauges can be installed before machine assembly, or where parts can be dismounted for strain gauge installation. In contrast to a cold-curing adhesive, the hot-curing adhesive offers a wider application range at higher temperatures, and is suitable for meeting the generally higher accuracy requirements in transducer production.

Select the Correct Glue for Your Strain Gauge

null

Important Information

It is essential not to use any adhesive other than the recommended one. Strain gauge adhesives must fulfill different requirements than general adhesives. This is why they are generally based on special developments or modifications of commercial adhesives. The simple adherence of a strain gauge to an object is not a sufficient criterion to evaluate the adhesive’s suitability for measurement purposes, it must also ensure the object’s strain’s faultless transmission. This requires more in-depth investigations (strain gauge tests according to VDI/VDE 2635 or comparable standards automatically include the adhesive).

Useful Temperature Range for Bonding Materials

null
null
Bonding material (adhesive)
Main application areas
Material
Useful temperature range (approx.) for zero-point related1) and for non zero-point2) related measurements3)
No. of components
X60, cold-curing (superglue) Experimental test Methacrylate 1)  -200°C …+60°C
[-328°F …+140°F]
2
2) -200°C …+60°C
[-328°F …+140°F]
1-CA80, cold-curing (superglue) Experimental test, transducer manufacturing with lower accuracy requirements Cyanoacrylate 1) -55°C …+100°C
[-67°F …+212°F]
1
2) -70°C …+120°C
[-94°F …+248°F]
X280, cold-curing  Experimental test  Epoxy resin  1) -200°C …+200°C
[-328°F …+392°F]
2
2) -200°C …+280°C
[-328°F …+536°F]
EP70, hot-curing  Experimental tests at elevated temperature range  Epoxy resin  1) -40°C …+70°C
[-104°F …+158°F]
2
2) -40°C …+70°C
[-104°F …+158°F]
EP310N, hot-curing  Experimental tests at elevated temperature range, transducer manufacturing  Epoxy resin  1) -269°C …+260°C
[-454°F …+500°F]
2
2) -269°C …+310°C
[-454°F …+590°F]
P250/P250-R, hot-curing Transducer manufacturing Phenolic resin 1) -196°C …+250°C
[-320°F …+482°F]
1
2)  -196°C …+250°C
[-320°F …+482°F]
P250 Stick-on, hot-curing Transducer manufacturing Phenolic resin 1) -196°C …+250°C
[-320°F …+482°F]
-  
2)  -196°C …+250°C
[-320°F …+482°F]
DP490, cold-curing Experimental Test Epoxy resin  1) -55°C …+120°C
[-131°F …+248°F]
2  
2)  -55°C …+120°C
[-131°F …+248°F]

1) With zero-point related measurement, the measured values are referenced to the zero point (usually static measurements).

2) With non zero-point related measurement, the zero point can fluctuate, only the dynamic part is important (dynamic measurement).

3) The specified temperature limits are fluid and depend on strain gauges being used, on the expected measurement accuracy and on the curing process.

Bonding material (adhesive)
Pot Life
Curing conditions
Suitable for strain gauges in series
Temp. 
Time 
Contact pressure
Y, C, M, D
G
A, U
E
X60,
cold-curing (superglue)
3 … 5 min 0°C [32°F]
20°C [68°F]
35°C [95°F]
60 min
10 min
2 min
Thumb pressure o o o
1-CA80,
cold-curing (superglue)
- 5°C [41°F]
20°C [68°F]
30°C [86°F]
10 min
1 min
0.5 min
Thumb pressure o o o o
X280,
cold-curing
30 min 20°C [68°F]
65°C [149°F]
95°C [203°F]
8 h
2 h
1 h
0.05 … 2 N/mm2

o

o

EP70,
hot-curing
2 hours 60°C [320°F] 3 h contact pressure B Series
EP310N,
hot-curing
4 weeks 150°C [302°F]
180°C [356°F]
200°C [392°F]
3 h
1 h
0.5 h
0.1 … 0.5 N/mm2

 •

 •

 • 

• 

P250/P250-R,
hot-curing
Unlimited 140°C [284°F]
160°C [320°F]
190°C [374°F] 
4 h
3 h
1 h
10 – 50 N /cm²
P250 Stick-on,
hot-curing
 - 140°C [284°F]
160°C [320°F]
190°C [374°F] 
4 h
3 h
1 h
10 – 50 N /cm²

 •

 •

 • 

DP490,
hot-curing
12 months 20°C [68°F] 
30°C [86°F] 
40°C [104°F] 
10 h
20 h
40 h
contact pressure

 •

 •

 • 

 •

•  Optimal combination of strain gauge and bonding material

o  Suitable, but sacrificing a part of the strain gauge or bonding material temperature range

–  Unsuitable combination


Mentioned Products

No more result to load