arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All Aqira See All Aqira - Test Data Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Structural testing of airframes with QuantumX at AVIATEST

AVIATEST, Latvia

Introduction

Aviation nowadays is one of the key transport industries carrying millions of passengers on a daily basis. Needless to say safety in the air is a top priority and Latvian company AVIATEST has been carrying out rigorous and comprehensive aircraft tests for decades. State of the art technology is of crucial importance in performing such sophisticated tasks and HBM's data acquisition system QuantumX is an integral part of the company's daily work. Back in the days of the Soviet Union, AVIATEST usually performed full-scale tests with a dozen of Soviet U-built planes and helicopters. Nowadays it’s all about the specialization - AVIATEST tends to focus on different longevity, resources and static strength tests. Established more than forty years ago AVIATEST now cooperates with aviation companies based in the European Union as well as Russia. Similarly to Latvian aviation as a whole, AVIATEST aims to serve as a bridge between the West and the East.

chevron_left
chevron_right

QuantumX has helped to make an extra step

Several decades ago the company used a system developed in the USSR, capable of performing static measurements only. When measuring dynamic parameters became a necessity, AVIATEST turned to different companies before finally choosing HBM thirteen years ago. In the pre-Quantum X era the number of sensors whose data was simultaneously obtained rarely exceeded 50. Now the company is capable of performing more difficult tasks. In some cases the number of sensors has even doubled. Along with the reduced amount of time necessary to gain data it is also the mobility and simplicity of Quantum X that is most valued at the company.

Aviation becomes more efficient and safer

To illustrate this better, AVIATEST is currently involved in a project called NICETRIP, which unites a couple dozen of European companies aiming to develop a civil tilt-rotor aircraft. In order to carry out the gearbox tests, the company uses 32 channels alone for router strain gauge measurements. In addition 70 other sensors are used for measuring temperature, pressure, stress, force and other indicators on the gearbox.

AVIATEST has also performed a number of flight tests which means QuantumX has literally taken off. One of the most impressive tests were of the world's largest helicopter that has ever went into production - Mi-26. The main task for AVIATEST was to measure stress analysis of its airframe.

Aviation industry becomes both safer and more efficient with more accurate and thorough tests that companies perform using modern technology like QuantumX. In the recent years AVIATEST has participated in testing aircraft before its first flight. Among them are Sukhoi Superjet 100, which is the first Russian designed and built regional jet, as well as Kamov Ka-62 and Irkut MS-21 that both haven't made their first flight yet.

The extent of cooperation with HBK has no limits

QuantumX is the sole module currently used at AVIATEST. Among many others the tasks performed with it range from elementary composite samples to fuselages with pressure testing as well as performing static tests of different components of airframe. The long cooperation with HBM has allowed AVIATEST to introduce a wide variety of HBM's products in their everyday use. Those include HBM load cells, certain amplifiers, strain gauges and the software as well. The successful cooperation between the two also means that AVIATEST is seeking to enhance it further. In the foreseeable future the company is likely to acquire additional strain gauges, load cells, modules, amplifiers and even torque meters that have been produced by HBM. AVIATEST is set to use yet another service provided by HBM as soon as it is about to get to the next stage of Irkut MS-21 tests. It has a capacity of approximately 2000 strain gauges in the airframe, thus the company plans on sending their staff to receive a certificate from HBM in order to install the strain gauges.

AVIATEST

The main activities of AVIATEST are full-scale airframe strength tests of fixed wing aircrafts, rotorcrafts, eVTOLs, UAVs and their main units. The other activity of AVIATEST is development, manufacture and supply of test equipment on a turnkey basis. The company designs and supplies a wide range of modern equipment, including multi-channel load systems and load control measurement systems.

The research and testing centre provides services for organising and accompanying the international certification of various aircrafts in accordance with EASA, FAA and other standards, but also performs structural and material tests for automotive, railroad and wind energy industries.

AVIATEST also successfully participate in various EU funding programmes like Horizon 2020, CLEAN SKY, CLEAN SKY 2 and CLEAN AVIATION.

More about AVIATEST

Technology used