arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All Aqira - Test Data Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

HBK Strain Gauges on Board for Type Certification of the Airbus A350 XWB

facc, CoLT, germany

Introduction

With the A350 XWB, Airbus brings a wide body aircraft to the market which sets new standards in terms of fuel savings and environmental friendliness. The assembly at the end of the wing consisting of the winglet and wing tip plays an important role, increasing speed as well as reducing the induced drag of the wing and consequently the fuel consumption. Both the wingtip and winglet assemblies are manufactured by FACC AG. The Austrian specialist for lightweight components delivers to Airbus not only these essential structural components of the new aircraft, but also takes necessary steps for the type certification of the aircraft through static and dynamic load tests.

chevron_left
chevron_right

Engineers were faced with unique challenges

The engineers were faced with unique challenges: in addition to the winglet/wingtip components themselves, the connection to the main wing box of the aircraft was also under test. Specifically for this purpose a dummy wing box with identical stiffness properties and connection concept was developed. In addition, the FACC AG subsidiary CoLT Prüf und Test GmbH has implemented a unique test rig for the testing of the Winglet assembly and dummy wing box. It enables the targeted synchronous initiation of a 3D deformation of the eight-meter long, fiber composite specimens. Equipment from HBK is also on board: CoLT relies on strain gauges from HBM to validate the measurement results of the static and fatigue tests.

New dimension in winglet testing

Over 125 tons, 15 meters long, ten meters high and eight meters wide - these are the impressive dimensions of the CoLT-built test rig for the Level 3 full-scale test of the A350 XWB winglet/wingtip. The implementation of five yokes each with three hydraulic cylinders allows for accurately controlled and synchronized loading of the specimens. For the first time, this enables static and dynamic continuous and peak loads on the over eight meter long elements to be determined under realistic conditions and their structural health monitored.

Validated for measurement results thanks to HBK

Within the context of testing and validation, the CoLT testing team relies on measurement technology from HBK. To ensure the best possible measurement results, only HBK strain gauges were used in the test rig. In total, over 550 flexible and easy to deploy HBK strain gauges were used in the Airbus A350-900 Winglet Wingtip Full Scale Certification Program - including 307 strain gauge rosettes 1 RY91-6 / 120 for the analysis of biaxial stress state with unknown principal stress directions and 257 linear strain gauges 1-LY41-6 / 120 to measure strain in one direction. Their task: validating the FEM calculation results required for type certification of the new Airbus model. During these tests, the HBK components confirmed the test engineers' positive experiences from the past. Even under challenging test conditions, they provided the expected precise measured values which confirmed the calculated interdependencies of component behavior. This completes another major step towards type certification.

Facts & Figures

  • Dimensions of the winglet test stand: 15 meters long, 10 meters high, 8 meters wide
  • Weight of the test stand: 125 tons
  • More than 550 strain gauges used

FACC

We are a global aerospace leader when it comes to designing, developing and manufacturing advanced aircraft components and systems for the global aerospace industries. 

More about FACC

CoLT

CoLT is a professional partner supporting product development and innovation.

CoLT has a strong history in the aviation industry, from which we draw a wealth of knowledge and experience in complex testing, enabling us to be adaptive and master complex tasks in various industries.

More about CoLT


Technology used