arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All Aqira - Test Data Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

SEAT Tests Vehicles Faster With HBK’s Autonomous DAQ System

SEAT, Spain

Introduction

Volkswagen Group specifications require that vehicles are tested during the development phase at SEAT in order to ensure that quality and durability standards are met. The challenge for the SEAT team was to set up a data acquisition (DAQ) system that is fast enough to provide more precise control over the instrumented parts and the entire data acquisition. The team developed an autonomous acquisition, communication and analysis process that meets all requirements – the ADAQ system. 

chevron_left
chevron_right

The Autonomous System

The car is shipped to a test track, where the test is carried out. The ADAQ system tranfers data to the headquarters daily, so the analysts can check and analyze the data. The system is started up, when the vehicle is turned on. It performs the following steps:

1. Boot up the catman software

2. Initiate data storage while the vehicle is on the road

3. Stop recording once the car is back at the circuit pit

The system reports irregularities to the analysts to enable them to take further action. The ADAQ is designed to warn the driver when an error occurs.

Together with the Polytechnic University of Catalonia, SEAT has developed a system for an Autonomous Data AcQuisition process, also called ADAQ. It is comprised of QuantumX DAQ modules, catman software and an electronic circuit that guarantees both the power supply for all devices and the vehicle-pilot interaction. The following DAQ systems and sensors were used: the QuantumX MX840B universal module, the MX1615B strain gauge module and one CX22B-W datarecorder, thermocouples, accelerometers, strain gauge bridges, displacement sensors, and, in addition, 14 CAN channels and GPS. Due to the wide range of conditions in which the vehicle is likely to be tested, the QuantumX equipment was securely mounted in the vehicle. 

Why Did SEAT Choose the HBK DAQ System?

  • Ability to work autonomously
  • Flexible and ideal for any test
  • Small, light-weight and easy to install
  • Designed to work in adverse conditions, e.g., vehicle fatigue tests (high vibration, relevant G force and extreme temperature)

catman was the software of choice for the ADAQ project, because it provides many different automation options. The setup includes the auto launch of catman, the auto loading of the acquisition project and the automated execution of the first DAQ job. Data files are recorded every 10 minutes. If an unexpected error occurs, the ADAQ system will record up to the moment the error is detected. So no data will be lost. The following filename format is used: XXXYYMMDDHHMMSS, with each letter corresponding to digits for project identification, year, month, day, hour, minute and second. The start and stop acquisition triggers use GPS parameters. This feature that provides greater precision requires three conditions to be specified for starting and stopping acquisition: latitude and longitude coordinates and vehicle speed (greater than 0 to initiate acquisition and equal to 0 when the test is completed).

Control Device Communicates with Driver

A control device (CD) has been designed to control the electronics and distribute power to each module. Besides the CD, a voltage rectifier and a driver control box have been installed. Thanks to the electronic circuit implemented and the use of CX22B-W digital outputs, four different statuses have been established in order to notify the driver of the different ADAQ phases. This is made possible by two LEDs installed on the vehicle dashboard.

Loading Software/Channel Error

Permanent red light: Informs the driver that the devices are booting and the project is loading, when the vehicle is switched on. If the red light comes on during acquisition, an error has occurred. The DAQ is stopped, the driver must go to the pit stop and report the problem.

Recording

Flashing green light: Informs the driver that data is being acquired and saved. Everything works fine. 

Ready to Record

Permanent green light: All devices are ready to initiate data acquisition. The project is waiting for the trigger to start recording data. The driver can leave the box area.

Event During Recording

Flashing red light: Occurs for different purposes. In this test vehicle it means that damper temperature is too high.

 

Autonomous Data Transfer and Analysis

Once the data has been recorded and saved to the CX22B-W memory card, it is uploaded to the SEAT server for subsequent computer analysis. Thanks to programmed commands and a previously configured AdHoc network, the CX22B-W is able to upload the data autonomously to another laptop in the circuit pit. This laptop sends the data to the SEAT servers overnight. A specific application will subsequently perform the analysis on the preselected channels and generate the required report - all totally autonomously. 

About SEAT

SEAT is one of the most well-known brands in Spain. Founded over 73 years ago, SEAT put Spain on wheels and shaped the lives of many for generations. The Spanish brand offers younger and first-time car owners a dynamic driving experience at an affordable price, without compromising on quality. SEAT is the brand with the youngest customer profile in Europe (10 years younger than the industry average).

More about SEAT

Technology used