arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management
null

Definition of a Pressure Sensor

In this article we explain the working principles and different types of pressure transducers and pressure sensors.

What is a Pressure Sensor?

  • Definition of Pressure as a Measured Quantity: Pressure is defined as the applied force by a liquid or gas on a surface and it is usually measured in units of force per unit of surface area. Common units are Pascal (Pa), Bar (bar), N/mm2 or psi (pounds per square inch).
  • Definition of a Sensor: A sensor is a device that measures a physical quantity and translates it to a signal. The quantity can be for instance temperature, length, force, or – of course – pressure. The signal is in most cases electrical but can also be optical.
  • Definition of a Pressure Sensor: Therefore, a pressure sensor is an instrument consisting of a pressure sensitive element to determine the actual pressure applied to the sensor (using different working principles) and some components to convert this information into an output signal.
null

Working Principles of Pressure Sensors


There is a variety of different technologies used within pressure sensors to provide accurate results. The following section will highlight some of these.
  • Strain gauge based pressure sensors also use a pressure sensitive element where metal strain gauges are glued on or thin film gauges are applied on by sputtering. This measuring element can either be a diaphragm or for metal foil gauges measuring bodies in can-type can also be used. The big advantages of this monolithic can-type design are an improved rigidity and the capability to measure highest pressures of up to 15,000 bar. The electrical connection is normally done via a Wheatstone bridge which allows for a good amplification of the signal and precise and constant measuring results. See our offer of strain gauge based pressure sensors.
  • Capacitive pressure sensors use a pressure cavity and diaphragm to produce a variable capacitor. The diaphragm is deformed when pressure is applied and capacitance decreases accordingly. This change in capacity can be measured electrically and is then set in relation to the applied pressure. These sensors are limited to low pressures of roughly 40 bar.
  • Piezo-resistive pressure sensors consist of a diaphragm – mostly made of silicon – with integrated strain gauges to detect strain as a result of applied pressure. These strain gauges are typically configured in a Wheatstone bridge circuit to reduce sensitivity and increase the output. Due to the material being used the pressure limitation is at around 1,000 bar.
  • Unlike the aforementioned technologies – which all use the deflection of a measuring body – resonant pressure sensors use the changes in resonance frequency in a sensing mechanism to measure stress caused by applied pressure. Depending on the design of these sensors, the resonating element can be exposed to the media, where the resonance frequency then depends on the density of the media. Sometimes these sensors are also sensitive to shocks and vibration.
Other pressure sensors that also do not use a measuring body can be thermal or ionization sensors, which use changes in thermal conductivity due to density changes in the flow of charged particles to measure the applied pressure.

Types of Pressure Measurements

There are a variety of properties that can be used to classify pressure sensors, including the pressure range they measure, the temperature ranges of operation, or the type of pressure they measure. Different pressure types can be absolute, gauge, sealed gauge, and differential pressure.
  • Absolute pressure sensors measure the pressure relative to a reference chamber (nearly vacuum).
  • Gauge pressure sensors – or relative pressure sensors – are used to measure the pressure relative to the currently present atmospheric pressure.
  • Sealed gauge pressure sensors are like a gauge pressure sensors, but they measure pressure relative to a fixed pressure rather than to the current atmospheric pressure.
  • Differential pressure sensors idetermine the difference between two pressures and can be used to measure pressure drops, fluid levels, and flow rates.
The obvious advantage of an absolute pressure sensor is to always measure against the same reference pressure (vacuum) and therefore be unaffected toby atmospheric pressure changes and less affected by temperature changes.

Pressure Sensors from HBM

HBM has over 65 years of experience in developing and manufacturing test and measurement equipment, including strain gauge-based pressure sensors. If you are looking for more information on our range of pressure sensors, please contact us.

Related Products

No more result to load