arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All Aqira - Test Data Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

HBK Supports Sikorsky in Complex Helicopter Testing

Sikorsky Aircraft Corporation, United States of America

Introduction

The ground test instrumentation team at Sikorsky faced the challenge of having multiple test scenarios, and many requirements for the complex testing systems utilized in the development of their helicopters. Their goal was to find a single data acquisition system fulfilling all their testing needs.

Sikorsky selected HBK as a partner to deploy a fleet of DAQ systems satisfying their requirements. A project team formed by the Sikorsky Ground Test Instrumentation personnel and HBK experts from the US and Germany analyzed the requirements and started the development of an overall system concept to solve the problem.

Problem

The helicopter is a complex machine, with a multitude of systems to be tested and qualified; consequently, the test lab has a range of very different test benches. It is an advantage to have a DAQ system that can operate in a range of test applications, and under numerous test scenarios rationalize multiple channels of data in a single file.

Solution

HBK identified QuantumX as the ideal DAQ system for Sikorsky's testing needs. This system is modular, scalable and with a flexible architecture, meets the requirements for an easily- and fast-reconfigurable system that supports an extremely wide range of sensors and transducers.

Result

The flexibility and scalability of the QuantumX data acquisition system from HBK now allows Sikorsky to use a single DAQ system to satisfy all their testing needs. The rapid reconfiguration capability of the QuantumX data acquisition system is ideal for use with all the test setups at Sikorsky.

chevron_left
chevron_right

Structural testing of a full-scale aircraft is always impressive to look at: complete fuselages and wing structures entangled in steel cages, subjected to extreme loads by dozens of actuators, incredible wing deflections and thousands of strain gauges and sensors. When it comes to helicopter testing, the game changes: even without leaving the structural field, requirements become very specialized and diversified. Unlike the fixed wing aircraft world, where most efforts in terms of data acquisition are aimed at full-scale test installations, a typical Helicopter test lab has a multitude of very different test benches.

The range of testing required

Rotating parts (hubs, tension links, shafts, levers etc.) represent an important effort in terms of component testing. Tests can vary from small, simple test benches such as a single pitch link in uniaxial load configuration to more complex test installations like a main rotor hub. An important portion of testing efforts focuses on blades. Main and tail rotor blades must be qualified with fatigue tests simulating the entire life cycle with an important safety factor. Helicopter blades randomly taken from production are converted into test articles, by adding the proper interfaces for test bench mounting. Since the applied loads are very high, blades are routinely tested in short sections to better handle load insertion and deflection.

null

Airframe testing is of very high importance. The fuselage is tested in full-scale configuration for fatigue and static test clearance. Large test structures, dozens of actuators and many thousands of strain gauges are common on this kind of test.

In certain cases, fuselage sections can also be tested separately on smaller test benches for more in-depth analysis.

null

Gearboxes and transmission are highly critical components. Dedicated test stands are set up to allow testing of the entire lifespan of a transmission, simulating loads coming from the rotor and extreme conditions such as over torques or oil leaks. Measurements in these areas tend to focus on torque, rotation, pressure and temperature. In addition, all actuators, hydraulic and control systems have a fundamental role in granting control of the machine and in no case should fail or malfunction.

This means that one of the most important testing scenarios features temperature, load and pressure measurements. On a slightly larger scale during Environmental test campaigns single components or even entire airframes may be tested in climate chambers to determine their response to extreme cold or heat. This is because it is crucial to ensure all the machine’s critical components remain efficient and responsive even under unpleasant environmental situations.

A Single Solution for Data Acquisition

Now imagine being an Instrumentation Engineer, receiving the task to specify a data acquisition system for a very large set of test applications required in the development of a helicopter. This was the challenge that the Sikorsky Ground Test Instrumentation Team faced. Many test scenarios, many requirements, and one target: find a single data acquisition system fulfilling all of this. Sikorsky turned to HBM as a partner for their new DAQ system. Therefore, a project team formed by the Sikorsky Ground Test Instrumentation personnel and HBK experts from USA and Germany analyzed the requirements and started development of an overall system concept.

In the design phase, there were some vital requirements stated by Sikorsky that would go on to play a major role in the final DAQ System definition.

  • The system must support all possible sensors and transducers used in the company’s laboratories, with individual per channel configurable sensor types, filters, and sample rates running on the embedded hardware. On top of that, digital avionics bus data need to be logged from MIL-STD-1553 and ARINC-429.

  • The data acquisition system must be accommodated in a specialized cabinet known as the Shell.

  • The shell has to be mobile, compact, of robust design, and offer an efficient interface with the data acquisition system. Ethernet and wireless connectivity are needed.

  • The shell must be rapidly reconfigurable by adding, removing or switching between measurement modules without needing tools, with a maximum reconfiguration time of 5 minutes.

  • Measurement modules must be able to operate outside the Shell, in the form of compact, portable DAQ systems.

  • The system must be able to interface with the company’s existing network infrastructure via wireless Ethernet connection, uploading data to share while the test is running.

  • The system must be able to interface with existing Sikorsky’s control systems and safety/shutdown systems, ensuring interlock connectivity and cycle counting capability.

QuantumX Data Acquisition System

QuantumX was the DAQ system HBM selected for this project. Its modular, scalable and flexible architecture met Sikorsky’s requirements perfectly. It is an easy- and rapidly-reconfigurable system, with the ability to support an extremely wide range of sensors and transducers.

Following testing and consultation the result of the Sikorsky-HBM joint development is a shell capable of housing 18 QuantumX modules. This allows a total channel count of more than 250 channels using high-density 16 channel modules. Each shell is a fully autonomous mobile data acquisition station. And by using the QuantumX CX22B-W Data Recorder, which runs HBM’s PC software catman®AP, this removes the need for an additional PC.

null

A Custom Made DAQ Station

null

The Shell features:

  • Light-weight movable cabinet
  • Top-mounted wide screen
  • Network manageable Uninterruptible Power System (UPS)
  • PTP capable Ethernet switch for networked operation
  • High-gain wireless connectivity
  • Watchdog functionality
  • Internal light, multiple brush strips, cable fastening supports
  • Sliding drawer, keyboard and touchpad
  • Lockable glazed rear door

With HBK's equipment, the Sikorsky Ground Test Instrumentation Team now deploys a fleet of DAQ systems satisfying all of their testing needs. The custom design allows unprecedented rapid reconfiguration for all of their different test setups. In addition, the software, catman®AP running on the CX22B-W data recorder features specific functions for fatigue testing such as cycle-based data recording and multiple parallel recorders.

Thanks to the flexibility and scalability of the QuantumX DAQ System, high channel count applications are now possible by linking multiple data system shells together, synchronizing thousands of channels and storing them in a single file.

Sikorsky

From the flight of the world's first practical helicopter in 1939, Sikorsky has remained the industry leader through its commitment to innovation, excellence and safety.

Sikorsky (a Lockheed Martin Company) provides military and rotary-wing aircraft to all five branches of the U.S. armed forces along with military services and commercial operators in 40 nations.

More about Sikorsky

Technology used