arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Aqira - Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All Aqira See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Metrological Traceability in Force and Torque Measurement

How to Shorten the Time for Comparison Measurements

Even if you are barely aware of it, metrological traceability is important to our daily lives. For instance, automotive construction is unthinkable without correct mechanical dimensions. Traceability ensures that a measurement result can be referred to or is related to a standard. A traceable measured value is related to this recognized standard by a continuous chain of comparison measurements with known measurement uncertainty. However, for each of these continued comparison measurements, the result of the comparison becomes “lower order”. Carefully selected measuring equipment can reduce this effect. Due to this reason, comparison measurements – whether they are international comparison measurements such as “CIPM key comparisons” or “RMO key comparisons” or multilateral or bilateral comparison measurements by accredited laboratories – must be performed with the utmost care.

To prepare a comparison measurement, a pilot laboratory with several years of experience, which has usually also requested the comparison measurement, develops what is called the “technical protocol”, defining the specifications for the measuring systems to be used. Finally, a measurement uncertainty budget must be available at each participating laboratory, which in turn depends on the measuring equipment utilized. Such comparison measurements are naturally very time-consuming, taking between two months to one year, depending on the type. Therefore, it is worth trying to reduce the time required.

It has become evident that transducers based on strain gauges (SG) have the lowest measurement uncertainties for the measured variables force and torque. Hence, they are used as reference transducers and transfer standards for comparison measurements.

TOP Transfer Force Transducers

As a manufacturer of measurement technology solutions, HBM has, over several decades, acquired the necessary specialist know-how to be able to offer reference measuring chains. The reference force transducers of the TOP-Z30A series are highlighted as representatives of the TOP transfer force transducers, which have been specially designed for international comparison measurements. The TOP-Z30A offers extremely high precision for both tensile and compressive forces and exceeds the requirements of the highest accuracy class 00 of the international standard ISO 376:2011, in part by up to a factor of 10. At the same time, the sensors have particularly high repeatability. The TOP-Z30A is available with TEDS, a type of electronic data sheet integrated with the transducer, as standard. TEDS (Transducer Electronic Data Sheet) enables data to be read directly into the measuring amplifier. If the transducer is sent from laboratory to laboratory during an inter-laboratory comparison, the time required to configure the measuring chain in the respective laboratory is significantly reduced.

null

TN Torque Transfer Transducer

null

HBM’s TN reference torque transducers are also optimized for international comparison measurements. In this case, the special challenge is that a monolithic design in shaft shape is required for comparison measurements. However, shaft sensors can only be designed as “open” sensors and not hermetically sealed, as it is the case with the better part of the strain gauge-based sensors. This poses the challenge of making the sensor immune to fluctuations in relative humidity. This is necessary even though the laboratories are air-conditioned since the sensor must be transferred from laboratory to laboratory.

The version used for the TN reference torque transducer shows such a low dependence on humidity that “climate adjustment” can be performed in the shortest possible time. This implies that the total time required to pass through all the laboratories, including the transfer time, can be reduced, however, the results still fulfil a certain measurement condition.

Precision Amplifiers

Since the signal coming from the Wheatstone bridge of a strain gauge-based transducer is extremely small, a bridge amplifier is always required to be able to finally display or process the result. Reference transducer and precision measuring amplifier together make up a precision measuring chain. The requirements placed on these precision measuring amplifiers are even higher than the requirements on the associated reference transducers.

HBM’s DMP41 precision amplifier is the most accurate amplifier for strain gauge-based measurements worldwide, rendering it ideal for international comparison measurements. It is the result of the development of the DMP series, which has been going on for more than four decades now; it impresses with its outstanding long-term stability and user-friendliness, such as touchscreen operation. The impact of humidity to sensitivity, as explained above, is also relevant to precision amplifiers: With an ever-decreasing measurement uncertainty budget, the influence of humidity can no longer be neglected. This knowledge was incorporated into the development of the device, and, hence, the DMP41’s sensitivity to humidity could be reduced by about another power of 10, compared with its predecessor device, the DMP40.

null

HBM's Expertise in Precision Measurement

Until 1992/1993 HBM’s 20 kN·m torque dead weight machine shown in the teaser image of this page played the role of a “national standard” in Germany, so to speak

Related Content

No more result to load