arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Optimizing Structural Health Monitoring Using Optical Technology

How can you ensure the safety and longevity of our infrastructure? The answer – by employing predictive and cost-effective infrastructure monitoring solutions that deliver reliable data on structural behaviour and status.

These solutions often consist of a combined usage of different technologies. HBM provides the entire measurement chain for these types of applications, from sensor to software, through the acquisition hardware.

In this webinar we will introduce you in how optical technology solutions are used to overcome challenges in structural health monitoring measurements. With the upcoming optical interrogator MXFS, optical technology is integrated into one of the most successful data acquisition platforms of HBM: the QuantumX. You’ll learn more about this powerful combination of the modular concept of QuantumX and its capabilities with the most wanted advantages of optical technology and how they benefit your measurement projects.

This webinar will discuss:

•    The common challenges of structural monitoring systems
•    How optical technology benefits such applications
•    The new optical interrogator from HBM, including its advantages, namely for infrastructure monitoring.

Date: 2020 May 13th

Instructors: Cristina Barbosa

Duration: 1 hour

Language: English

Black and white portrait of Cristina Barbosa, Product Manager Optical Business at HBK FiberSensing
Cristina Barbosa
 

Product Manager Optical Business

Questions from Webinar Participants Answered by Cristina Barbosa

HBM FiberSensing supplies cables with several FBG strain and/or temperature sensors.

Yes, HBK currently offers off-the-shelf solutions based on FBG for measuring strain, temperature,  displacement, tilt and acceleration.

Learn more

Yes, we have projects running in India for structural health monitoring using Fiber Bragg Grating technology.

Yes. We have teams within HBK who can support installation almost worldwide.

Sensors embedded in concrete do need special care during installation namely because:

  • Sensors have to be installed at a late stage of the construction work on the structure (as close as possible to the concreting operation), which means that they have to be installed while regular construction work is occurring the timing is usually critical and quite intense.
  • Sensors and cables are fragile items and workers must be aware of their existence and take this fragility into account.
  • Concrete pouring is a tough process, depending on the type of concrete and on the method used.

So, regarding the sensor location, care must be taken to prevent damage resulting from the whole process, for example:

  • Using a tight net to cover the sensor will ensure that large aggregates from the concrete mixture will not hit the sensor.
  • Using the vibrator at safe distances away from the sensor will ensure that the vibration process does not harm the sensors.
  • Embedding the sensor location in concrete in advance of the whole operation allows a controlled process over the sensor.

Care must also be taken with the cable paths, and we always suggest the use of tubes to protect the cables.

In addition, you must pay attention to where the cables exit from the concrete.

Again, several strategies can be used, and care is needed in all of them especially when removing the formwork to ensure that cables are not damaged by the process. A damaged cable close to its exit from the concrete is impossible to repair.

The QuantumX MXFS is compatible with FBG-based sensors from any supplier, as long as these are not based on special FBG’s (for example: phase-shifted FBG, long period FBG).

It measures peaks with different reflectivity, within the available dynamic range.

catman 5.4.1 is the first version of catman to support the QuantumX MXFS Interrogator.

Find out more

At the moment, QuantumX MXFS is compatible with catman AP but not with catman Enterprise. Please contact HBM if you have the need for this compatibility.

The QuantumX MXFS BraggMETER module has two acquisition rates that can be configured by the user: 100S/S and 2000S/S. On top of the set acquisition rate, different sampling rates can be defined on the device by down sampling.

The acquisition rate defines the sweeping speed of the laser as one complete sweep on the overall wavelength spectrum is needed for each sample.

The sampling rate corresponds to the number of samples that are made available which is also user definable.

No. The stated sampling rate is the same despite the number of sensors that are connected. All sensors can be acquired simultaneously and in parallel at the maximum acquisition rate.

The optical interrogators from HBK (DAQ) need to be connected to a PC for configuration and data saving. However, there are models, that can then be disconnected from the PC and operate as standalone and record data internally (FS22 Static).

Check for further details on our product page FS22 Industrial BraggMETER.

This is a tricky question to answer as it depends on the type of sensors and the structure being monitored. However, in our experience, for a system mainly consisting of strain and temperature measurements, and a structure that is regular and does not require special protection, or involve long distances, this number would be around 60 measuring points.

Optical sensors are available with different types of cables providing different levels of protection, and dependant on the environment, they might require further protection. For example, for cables embedded in concrete, it is advisable to use flexible tubes for the cable path; for cables deployed on a surface inside a bridge deck, a flexible tube, half a cane or a cable path tray could all be suitable solutions.

Related Pages