Validating Motors, Inverters, and Electric Powertrain using eDrive and Opal RT Power Hardware in the Loop

 

This webinar has been recorded and was originally held on December 8th, 2021.

One of the challenges while developing electric powertrains is how to validate and optimize components/Unit Under Tests (UUT). Development requires time consuming testing and significant capital investment for test stands. Power Hardware in the Loop (PHIL) systems can be an efficient way to validate motors and inverters with precision, saving cost at the later stages of the development cycle (certification for example). In a PHIL test, a real UUT is interreacting with one or more simulated components via real power flow. Anything (Motors, Grid, Inverters) can be simulated on a simulator, which controls the power amplifier that interfaces with the UUT. Once this validation is complete the UUT can then be moved to the full powertrain testbench (with no simulation).

This session will show how HBK’s eDrive system and Opal RT’s real time simulators can be used in a PHIL system to emulate motors effectively for the study of motor control methods – the motor and it’s control are simulated on an OPAL-RT simulator controlling the power amplifiers that interface with the grid. HBK’s eDrive system is used as the acquisition tool that is relied on in the PHIL system, and the real system with the real motor and dyno.

• What is a PHIL system?
• What are some PHIL configurations?
• How can PHIL save time?
• PHIL Case Study

 

Speaker:

Mitch Marks

Business Development Manager - eDrive

Contact: 

[email protected]

 

Reef Hamadah

Technical Sales Specialist, Opal-RT Technologies

Contact: 

[email protected]

Contact us Please send a message and a representative will contact you shortly.
Get a quote now!

Ask your HBK Sales Engineer

Please send me


Continue

Ask your HBK Sales Engineer

Please send me


Continue

Green check mark Individual offer

Green check mark Technical advice

Green check mark Fast response