Structural Health Monitoring
HBK's modular and scalable monitoring solutions, complemented by our competent support and service, save time and money, provide valuable insights, and help to increase the structure’s service life and safety.
How can you ensure the safety and longevity of our infrastructure? The answer – by employing predictive and cost-effective infrastructure monitoring solutions that deliver reliable data on structural behaviour and status.
These solutions often consist of a combined usage of different technologies. HBM provides the entire measurement chain for these types of applications, from sensor to software, through the acquisition hardware.
In this webinar we will introduce you in how optical technology solutions are used to overcome challenges in structural health monitoring measurements. With the upcoming optical interrogator MXFS, optical technology is integrated into one of the most successful data acquisition platforms of HBM: the QuantumX. You’ll learn more about this powerful combination of the modular concept of QuantumX and its capabilities with the most wanted advantages of optical technology and how they benefit your measurement projects.
This webinar will discuss:
• The common challenges of structural monitoring systems
• How optical technology benefits such applications
• The new optical interrogator from HBM, including its advantages, namely for infrastructure monitoring.
Date: 2020 May 13th
Instructors: Cristina Barbosa
Duration: 1 hour
Language: English
Product Manager Optical Business
HBM FiberSensing supplies cables with several FBG strain and/or temperature sensors.
Yes, HBK currently offers off-the-shelf solutions based on FBG for measuring strain, temperature, displacement, tilt and acceleration.
Yes, we have projects running in India for structural health monitoring using Fiber Bragg Grating technology.
Yes. We have teams within HBK who can support installation almost worldwide.
Sensors embedded in concrete do need special care during installation namely because:
So, regarding the sensor location, care must be taken to prevent damage resulting from the whole process, for example:
Care must also be taken with the cable paths, and we always suggest the use of tubes to protect the cables.
In addition, you must pay attention to where the cables exit from the concrete.
Again, several strategies can be used, and care is needed in all of them especially when removing the formwork to ensure that cables are not damaged by the process. A damaged cable close to its exit from the concrete is impossible to repair.
The QuantumX MXFS is compatible with FBG-based sensors from any supplier, as long as these are not based on special FBG’s (for example: phase-shifted FBG, long period FBG).
It measures peaks with different reflectivity, within the available dynamic range.
catman 5.4.1 is the first version of catman to support the QuantumX MXFS Interrogator.
At the moment, QuantumX MXFS is compatible with catman AP but not with catman Enterprise. Please contact HBM if you have the need for this compatibility.
The QuantumX MXFS BraggMETER module has two acquisition rates that can be configured by the user: 100S/S and 2000S/S. On top of the set acquisition rate, different sampling rates can be defined on the device by down sampling.
The acquisition rate defines the sweeping speed of the laser as one complete sweep on the overall wavelength spectrum is needed for each sample.
The sampling rate corresponds to the number of samples that are made available which is also user definable.
No. The stated sampling rate is the same despite the number of sensors that are connected. All sensors can be acquired simultaneously and in parallel at the maximum acquisition rate.
The optical interrogators from HBK (DAQ) need to be connected to a PC for configuration and data saving. However, there are models, that can then be disconnected from the PC and operate as standalone and record data internally (FS22 Static).
Check for further details on our product page FS22 Industrial BraggMETER.
This is a tricky question to answer as it depends on the type of sensors and the structure being monitored. However, in our experience, for a system mainly consisting of strain and temperature measurements, and a structure that is regular and does not require special protection, or involve long distances, this number would be around 60 measuring points.
Optical sensors are available with different types of cables providing different levels of protection, and dependant on the environment, they might require further protection. For example, for cables embedded in concrete, it is advisable to use flexible tubes for the cable path; for cables deployed on a surface inside a bridge deck, a flexible tube, half a cane or a cable path tray could all be suitable solutions.
HBK's modular and scalable monitoring solutions, complemented by our competent support and service, save time and money, provide valuable insights, and help to increase the structure’s service life and safety.
Suitable for large-scale sensing networks, HBK's optical interrogators provide precise and high-resolution static and dynamic measurements 24/7 through reliable software interfaces. They are specifically designed to measure the values generated by Fiber Bragg Grating (FBG) sensors.
HBK offer engineering training courses to help you develop the knowledge and skills needed to address challenges such as fatigue, reliability and durability analysis, sound, vibration and test measurement. Find out the courses to get you started.