Output resistance

This is the resistance present on the wires connected to the amplifier input. When connected in parallel, the output resistance's tolerance should not exceed 10 ohm; otherwise cross currents could affect the measurement result.

Force Measurement Glossary: Characteristics of Force Transducers

Benefit from our practical on-line glossary to look up the most important technical terms in the field of force measurement:

Kontakta Här kan du kontakta oss för att få veta mer om vad HBM kan erbjuda dig.