arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All Aqira - Test Data Management See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Data Acquisition & Analysis See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Case study: How HBK measurement technology helped Trasko Automatyka Sp. z o.o. develop an assembly line immune to electromagnetic noise

Trasko Automatyka SP. z.o.o., Poland

Introduktion

Did you know that HBKs measurement technology consists of a special shielding concept, making it immune to electromagnetic interferences of any kind? By using the special shielding concept from HBK, Polish automation company Trasko Automatyka Sp. z o.o. was able to develop an assembly line with torque control units providing safe and clear results for quality control. In a previous setup using equipment from other suppliers, this assembly line was heavily affected by electromagnetic noise causing severe problems for the end-of-line quality control.

chevron_left
chevron_right

A consistent shielded system

By facing the task of re-building and re-designing the assembly line, Trasko Automatyka Sp. z o.o. did a full review and check of the control systems used. One big challenge was the creation of a consistent system, considering the many parts, devices, control units, robots and mechanics used. For the measurement systems used, this means that they should be well shielded but not emit electromagnetic noise from themselves. The strong influence of electromagnetic noise on the torque measurement results caused by missing accuracy of the sensor as well as insufficient shielding can be seen in this chart:

null

The Greenline shielding design

By using the HBK measurement technology with its special shielding concept against electromagnetic interferences, Trasko Automatyka Sp. z o.o. was able to set up a process control system providing reliable results. They used the following setup:

  • A T20WN torque sensor for measuring signals
  • The PMX signal conditioning system for production control
  • The catman software for measurement visualization and analysis
  • Special double-shielded cables to connect the different parts of the measurement chain.

Protecting measurement systems against electromagnetic interference has been a long-time specialty of HBK products. For example, all electrical/electrotechnical components of the complete measuring chain are tested and technical safety issues are analyzed in HBK’s accredited in-house laboratory, thus ensuring that all normative requirements are satisfied.

Finally, a decisive factor for successfully building an “immune” measurement chain in the assembly line was the use of a special shielding design (“HBK Greenline”), ensuring safe and failure-free operation. Greenline-protected equipment neither emits any disturbances into the environment nor excessively loads the mains power supply. Using this setup, the complete measuring chain is fully enclosed in a Faraday cage through the unique design of the cable shield. The cable shield is flattened, connected to the transducer housing, and routed to the amplifier housing through conductive connectors. These measures substantially reduce the effects of electromagnetic disturbances.

Following are practical hints on how to ensure the shielding design: All components of the measuring chain (including all cable joints, such as connectors and couplings) have to be surrounded by a closed, EMC-tested shield. Shield transitions must be realized in the form of flattened, closed and low-impedance joints. This is ensured if original HBK connectors are used.

An important feature is the separate shielding covering the wires for the sensor and the second shielding for the amplifier. To gain perfect EMI protection, the amplifier as well as the second shield have to be connected to the ground. This guarantees a complete separation from the EMI. This principle is stated in the HBK “Greenline Concept” as a fundamental design for robust and secure measurement.

null

Safe and stable measurement results with HBK

Thanks to the introduction of a solution based on HBK’s products, customers gain certainty and get back the quality check on the highest level. The PMX amplifier proved itself in harsh environment with electromagnetic interferences and guaranteed reliable measurement results and improvement of production’s results.  A variety of control-measurement electronics occurs in an industrial environment, and thus, electromagnetic interferences force usage of equipment which fulfils the requirements of standard [1] for immunity and emission regarding the electromagnetic compatibility of electrical devices working at voltage lower than 1000V AC or 1500V DC used in industrial processes. The additional aspect interfering the work of devices is also the usage of data transfer on Wi-Fi, Bluetooth, RFID etc. interfaces that leads to interferences in radio frequencies within a range of 9 kHz up to 400GHz. The operation in such ranges of frequencies also leads to electromagnetic interferences. To fulfil those requirements, one should choose a control-measurement equipment which has test certificates of EMC standards.

Company

TRASKO Automatyka is a company based in Poland which deals with the production of machines for broadly understood industrial automation and with the design and implementation of electrical and teletechnical installations.

The company employs highly specialised, experienced personnel of engineers, mechanics designers, control system designers, programmers and assemblers. Their multiyear experience in the branch of mechanical engineering and system integration causes that the implemented solutions are transferred into the clients’ needs and satisfaction.

Technology used

Other case studies