HBM의 전력 분석 지식 포탈

HBM eDrive Testing은 인버터와 전기 구동 장치의 효율을 분석하는 전력 분석기입니다. 여타의 다른 분석기와 달리 전력화용으로 설계된 HBM eDrive Testing 솔루션을 사용하면 6상 기계에서 측정 데이터뿐만 아니라 심층 분석까지 며칠이 아닌 단 몇 초 안에 확인할 수 있습니다.


동영상

본 영상에서는 HBM의 eDrive Testing 전력 분석기와 그 작동 방식에 대해 자세히 설명합니다.

 
HBM eDrive Testing: Analyze Electrical Machine Data in Minutes
 
eDrive Testing: Explained by a user
 
Steinbeis Award for eDrive

백서(White Papers)

이메일주소를 등록하시면 eDrive에 관련된 모든 백서, 웹 세미나, 동영상을 무료로 볼 수 있습니다. 

Measuring the Parameters of a Transformer Equivalent Circuit Diagram

Used in many different applications, the transformer is one of the most important components in alternating current technology. It is used in electrical energy technology to transform between different voltage levels. To ensure efficient transmission of energy in this case, good efficiency and optimum utilization are required.

Qualification and Verification of High Power Battery Systems

Before a traction battery is introduced in the market, a qualification and verification of those systems is inevitable. A suitable test bench has to cover a high voltage and current range as well as a high dynamic and it should be able to execute the necessary tests as realistically as possible and in an application-oriented manner.

Calculating Power Quantities with Perception Software

Accurate and highly dynamic power measurements are required for assessing and testing electrical drives in industrial applications, and for hybrid and electric vehicles. This article considers the most important power values, along with some examples.

Efficiency and Loss Mapping of AC Motors

Recently electrical machines have become an important topic in many industries including power generation, heating/cooling, transportation and home appliances. With increases in efficiency standards and the increase in battery powered devices, the motor efficiency has become an important topic.

Getting the Back Emf Voltage Constant of Permanent Magnet Motors with Just One Lap Wrist Using

The parameter identification of permanent magnet motors is needed when a new motor prototype must be quickly analyzed. The parameter identification can be performed with complicated tests using inverter and a driving machine, or using simpler methods that do not need any inverter supply and prime movers.

Power Measurements on a 6-Phase Motor

The evaluation and testing of electric drives along with the corresponding control strategies in industrial and electrical mobility applications require precise and highly dynamic power measurements.

Power Measurements on a Pulse Width Modulated Inverter with Perception Software

Accurate and highly dynamic power measurements are required for assessing and testing electric drives in industrial applications, and for hybrid and electric vehicles. To be able to evaluate these measurement results, the function and working method of the drive components must be considered.

Measurement of Resolver Position Using Genesis HighSpeed Data Recorders

The resolver is an electrical machine that is intensively used in synchronous motor drives to measure the rotor position that is needed for the motor control algorithm. Due to its robustness, the resolver is the popular choice in harsh environments, where the electrical motor is subjected to mechanical stresses and vibrations, such as automotive and aerospace applications.

Calculating Space Vector Quantities and the Air-Gap Moment of Asynchronous Motors

Genesis HighSpeed data recorders from HBM are particularly suitable for measurements on inverter-fed AC induction motors. Thanks to their modular design, these measurement systems allow any number of channels while providing high sampling rates.

Calculation and Realization of Measured Quantities in Electrical Energy Technology as Space Vectors with HBM Perception Software

Space vectors are frequently used for clear and concise realization of measured quantities in electrical energy conversion systems such as transformers or induction motors. Additional information regarding the operating state of these energy converters can be determined if the time-dependent space vectors are realized as locus curves in the complex plane.

Measurement of Symmetrical Components in Three-Phase Systems

The growing proportion of renewable energy requires these energy producers to also achieve high reliability and defined behavior in critical operating situations. The symmetrical components method can be used to assess and evaluate the operating points of renewable energy producers.


어플리케이션 개요

HBM 전력 분석기의 고급 기능들에 대해 알고자 하시면 본 영상을 확인하세요.

 
Understanding the dq0 transform with the HBM eDrive Power Analyzer
 
Explaining a space vector control

웹 세미나(Webinars)

회원 가입(이메일 등록)후 로그인하시면 HBM의 eDrive Testing과 전자 기기용 전력 분석에 관한 모든 웹 세미나를 무료로 확인하실 수 있습니다.

Power measurement on wind turbine generators
This webinar explores how to determine and increase efficiency of wind turbine generators
Efficiency Testing on Electrical Drive Trains (US)
In this webinar we explain what is key to testing electric motors and inverters in the electric drive train.

성공 사례

eDrive Testing 시스템을 어떻게 사용할 수 있을까요? 여기서 eDrive 시스템을 사용한 응용 사례와 그에 대한 사용자들의 평가를 볼 수 있습니다. 


관련 제품

eDrive Testing: 차세대를 위한 eDrive Testing
보다 신속한! 더욱 정확한! 전기차 구동 효율 측정을 원하십니까?
Perception
Perception은 고속 데이터 수집을 위한 소트프웨어 패키지이자 측정 순서에 따른 모든 업무를 완수합니다.
1:1 문의 이곳을 클릭하셔서 요청사항을 작성해 주세요