Load cells ensure high accuracy in latest Weigh Blending Systems
TSM Control Systems of Dundalk in Ireland is using HBM’s single point load cells to ensure high accuracy in its range of Weigh Blending Systems.
TSM Control Systems of Dundalk in Ireland is using HBM’s single point load cells to ensure high accuracy in its range of Weigh Blending Systems. The Weigh Blending Systems measure a recipe of different plastic granules by weight and then blend the resulting mix so that it can be used in different types of plastic processing. Examples include packaging material such as food wrap or the internal wrapping bags in cereal boxes used in the food industry.