Title | Description | Date | Version | Related Documents |
Perception Software 64-bit | This is a major release of Perception. Due to the fixes, please download the release instead of Perception 8.54. | 01/2024 | 8.60 | Release Notes |
Perception Software 64-bit | This is a minor release of Perception mainly improving stability, fixing known problems and adding minor new features. Note: Needed if Perception has to get upgraded from a version below 8.28 before installing latest Perception version |
07/2022 | 8.28 | Release Notes |
This is a major release of Perception.
Bug Fixes
New Features for e-Power Suit:
New Features for Hardware:
Improvements on Perception
Improvements on Hardware
This is an minor release of Perception mainly improving stability, fixing known problems and adding minor new features.
This is not shipped out with the hardware but only available via web download.
Details about fixed issues and new features can be found in the release notes.
Note: Perception includes the instruments firmware for GEN DAQ systems. So there is no separate firmware available for GEN DAQ systems.
When you connect to hardware using a new version of Perception, the firmware in the hardware will be upgraded accordingly to the same release level.
Title | Description | Date | Version | Related Documents |
Perception CSI - Data Sheet | Perception CSI specifications | 12/2011 | ||
Perception CSI training - Data Sheet | Perception CSI training specifications | 12/2011 | ||
Perception CSI How to get started | This document describes what you need to create your own Perception CSI extensions. | 05/2019 | ||
CSI Examples | Examples used in the CSI Programming User Manual | 09/2020 | 6.0 | |
Perception Help File | Perception Programming Interfaces Help file | 05/2019 | 2019 | |
Perception CSI Sheet Project Template.vsix | Perception CSI Sheet template file for Visual Studio 2017 and later | 06/2022 | 5.0 | |
Perception.ScriptAction.Template.vsix | Perception CSI script action template file for Visual Studio 2017 and later | 06/2022 | 5.0 | |
Perception and GEN series: CSI Programming - User Manual | User manual Perception CSI programming | 03/2020 | 5.0 |
Title | Description | Date | Version | Related Documents |
Perception CSI: Sensor Barcode Reader - HOTnote | Perception CSI: Sensor Barcode Reader - HOTnote | |||
Perception CSI: Seismic Measurement - HOTnote | Perception CSI: Seismic Measurement - HOTnote | |||
Word Organizer Demo Files | Demo files which can be used by the Perception Word Organizer | 11/2010 | 1.0 | |
Perception CSI Extension - Datasources ASCII Export - User manual | 06/2009 | 1.0 | ||
Harmonic Analysis Sheet- User manual | User manual Harmonic Analysis Sheet | 06/2020 | 4.0 | |
Time Markers Table User Manual | User manual Time Markers Sheet | 06/2011 | 1.0 | |
Calculator Sheet User Manual | User manual Calculator Sheet | 06/2022 | 3.0 | |
Word Organizer Sheet User Manual | User manual Word Organizer | 06/2022 | 2.0 | |
Log File Reader User Manual | User manual Log File Reader | 06/2022 | 2.0 | |
Perception CSI Extension - Seismic Measurement - User manual | 06/2022 | 1.1 | ||
Calculator Sheet Trial Version | Calculates and displays statistical information of recorded data. Alarm levels can be used to color individual calculated results | 06/2022 | 3.4 | |
Time Markers Table Trial Version | Shows all time markers including triggers in a table. Can be used for navigating in Perception Display to specific trigger. | 06/2022 | 2.1 | |
Perception CSI Harmonic Analysis Sheet Trial Version | Calculate the amplitude of the harmonic components of a periodic signal using the Fourier series. | 06/2022 | 4.1 | |
Log File Reader Trial version | Reading back Perception Logged data into a Perception User Table. The data can be filtered and the layout can be adjusted | 06/2022 | 2.1 | |
Word Organizer Sheet Trial Version | Create a new Word or PDF report by assemble existing Word documents generated during a recording. Also bitmaps or richtext files can be added | 06/2022 | 2.1 | |
Drop-down functions User manual | 08/2022 | 1.0 | ||
Perception STL Verification Sheet | Sheet works with Perception 8 or later and explains the working of the STL formulas. The sheet can be used to verify the STL calculations on user data. | 03/2023 | 3.7 |
Title | Description | Date | Version | Related Documents |
Perception Remote control - Data Sheet | ||||
Perception remote control using LabVIEW - User Manual | 10/2012 | |||
Perception remote control using DIAdem - User Manual | Perception RPC using DIAdem | 10/2015 | ||
Perception remote control using LabView Demo source code | LabView source code of the Perception remote control Demo | 06/2019 | ||
Perception remote control using LabView Demo | LabView Demo program using the Perception RPC interface | 06/2019 | ||
Perception COM-RPC.msi | Installer of the RPC COM wrapper and RPC documentation | 06/2019 | 7.40 | |
Perception Remote Control RPC Demo | Simple Perception RPC demo program | 06/2019 | 1.3.19169 | |
Perception Remote Control RPC Demo Source code | C# source code of the Perception RPC Demo | 06/2019 | 1.3.19169 | |
Perception remote control using MATLAB - User manual example files | Perception RPC using MATLAB example code | 06/2019 | ||
Perception RPC/COM Interfaces Helpfile | Programming Help file Perception RPC/COM interfaces | 06/2019 | 7.40 | |
Perception Matlab® Remote Control - User Manual | ||||
Perception Remote Control RPC ePower Demo Source Code | C# source code for the Perception RPC ePower demo program | 09/2020 | 2.0.20251 | |
Perception Remote Control RPC ePower Demo | Simple Perception RPC ePower demo program | 09/2020 | 2.0.20251 | |
Perception Remote Control RPC ePower Demo | Simple Perception RPC ePower demo program | 09/2022 | 2.1.22252 |
Title | Description | Date | Version | Related Documents |
PNRF Reader Toolkit - User manual | PNRF Reader User manual | 07/2009 | 1.1 | |
PNRF Reader Toolkit- MATLAB example manual | PNRF Reader Example manual on how to read PNRF data files into MATLAB | |||
PNRF Reader Toolkit - Training material | PNRF Reader Training material documentation and code examples | 11/2021 | ||
Export PNRF Applic. - User Manual |
Title | Description | Date | Version | Related Documents |
GEN DAQ API C source archive (*.gz format) | Archive containing examples, help file and required source code for the ‘C’ interface. | 08/2020 | 4.0 | |
GEN DAQ API Installer for Windows | Running the install will copy all examples, help files and source code available for the GEN DAQ API to the PC. The install contains files for both the .NET and ‘C’ interface. The files will be installed to: C:\GEN DAQ API. | 01/2023 | ||
GEN DAQ API Installer for Windows | Running the install will copy all examples, help files and source code available for the GEN DAQ API to the PC. The install contains files for both the .NET and ‘C’ interface. The files will be installed to: C:\GEN DAQ API. | 05/2023 |
Title | Description | Date | Version | Related Documents |
GEN7tA - User Manual | 12/2016 | 2.1 |