A detailed description about your data recorder can be found in the CX22 user manuals:
Stand-alone recording
With the CX22 Data Recorder you can do stand-alone measurement without connecting any PC.
With the pre-installed catman software you can do interactive testing with a variety of visualizations for all different signals. In the unattended mode it is also possible to do black-box recording using a hugh set of different trigger options.
CX22 data recorder
The data recorders offer various interfaces like a standard PC and is the core of the system running the DAQ software catman. It is available in
CX22 operation
All CX22 Data recorders can work stand-alone or also act as a gateway to the PC.
In the stand-alone mode you have the option between a local operation by connecting a (touch-) screen, mouse, and keyboard.
It's also possible to connect a PC via Ethernet (cable or Wi-Fi) and to control the data recorder via a remote desktop session. The default user and password are shown in the manual, we recommend changing the password via the shell after first log-in.
It is also possible to work with local or remote operation as with any other PC with catman DAQ software in the interactive test mode.