Measurement of Resolver Position using Genesis HighSpeed Data Recorders

The resolver is an electrical machine that is intensively used in synchronous motor drives to measure the rotor position that is needed for the motor control algorithm. Due to its robustness, the resolver is the popular choice in harsh environments, where the electrical motor is subjected to mechanical stresses and vibrations, such as automotive and aerospace applications. The measured position is usually obtained through a resolver-to-digital converter that implements in a single chip several blocks, such as a signal demodulator, a voltage-controlled oscillator and a tracking loop. This work presents a method to obtain the position measured by a resolver using the high-speed voltage acquisition channels of HBM Genesis HighSpeed data recorders, with no requirement of additional hardware.

Related Products

Power Analyzers
HBM eDrive testing consists of two components – the power analyzer and DAQ system which are used to test electrical drives.
Kontakta Här kan du kontakta oss för att få veta mer om vad HBM kan erbjuda dig.