Save money with software maintenance contracts for catman

HBM Test and Measurement (HBM) offers an attractive package for its customers with multi-year maintenance contracts for catman data acquisition software.

Effective immediately, HBM is offering multi-year maintenance contracts up to five years for its catman data acquisition software. In this way HBM can ensure its customers will have direct access to technical support. New versions will be available at no cost within the covered period and customers will also be proactively informed of updates.

HBM has developed some important innovations in the most recent versions to boost measurement efficiency and ensure that customers' needs will be met in the future. A function library for electrical power is available. Wheel force sensors can be integrated and catman allows for data acquisition with synchronous recording of up to 4 camera signals. Users can export visualizations of processed measurement data to MS Word or MS Excel automatically to create reports. Numerous new storage and export formats are also available for other commonly used software packages for post processing. Classifying (Rainflow and Time-at-Level) can be done online and in post processing. The user can use autosequences to automate processes, for example performing automated assessments of tests with scripts.

1:1 문의 이곳을 클릭하셔서 요청사항을 작성해 주세요